Manufacturer Part #
597-3121-207NF
597 Series Red 2.4 mm 120 20 mcd Water Clear 1.75 V LED PLCC-2 Surface Mount
Dialight 597-3121-207NF - Product Specification
Shipping Information:
ECCN:
PCN Information:
Description of Change:Orientation and Polarity Marking of LED has changed.The new Red LED Pin 1 is Cathode and Pin 2 is Anode (same as old LED pin out).On the new Red LED, location of Polarity Mark was changed to Pin 1 Cathode Side.On the tape and reel packaging, the Pin 1 Cathode with Polarity mark is facing towards the sprocket.Reason for change:The change in polarity marking and orientation in the tape and reel packaging was done to make the packaging standardized for our PLCC-2 LEDs.
REVISION:Pls find the attached file to revise the plant move date for the Dialight Penang, MYS location. 1/12/2024: Revised test on cover sheet Added additional page listing affected part numbers4/18/2024: Updated key dates Based on revised information from MalaysiaNEW ADDRESS:Dialight Penang Sdn Bhd No.1478B,Lorong Perusahaan Maju 8, Kawasan Perusahaan Perai, 13600 Perai,Pulau Pinang, Malaysia.Change Description:Moving the existing facility in Penang, Malaysia to a new facility in Penang, Malaysia 2 blocks (150 m) away. There will be no change to current BOMs, standard operating procedures, staffing or equipment. New building configuration will allow for all production lines to be moved to the mew facilities and maintain the exact layout of production lines as the current building. The new site will be fully qualified by Dialight Operations, Engineering and Quality teams. Reason:Lease on existing building expiring. Move to new facility 2 blocks (150m) away required to provide improved efficiencies and capacity utilization to better support Dialight component's customers demands.
Change Description:Moving the existing facility in Penang, Malaysia to a new facility in Penang, Malaysia 2 blocks (150 m) away. There will be no change to current BOMs, standard operating procedures, staffing or equipment. New building configuration will allow for all production lines to be moved to the mew facilities and maintain the exact layout of production lines as the current building. The new site will be fully qualified by Dialight Operations, Engineering and Quality teams.Reason:Lease on existing building expiring. Move to new facility 2 blocks (150m) away required to provide improved efficiencies and capacity utilization to better support Dialight component's customers demands.The new address for the new MYS plant is as below : Dialight Penang Sdn Bhd No.1478B,Lorong Perusahaan Maju 8, Kawasan Perusahaan Perai, 13600 Perai,Pulau Pinang, Malaysia. The move will take place end of March into April of 2024.
Part Status:
Available Packaging
Package Qty:
2000 per Reel