Référence fabricant
LF07WBJ-6S
Connector JACK WATERPROOF 6 Position FEMALE
Hirose Electric LF07WBJ-6S - Spécifications du produit
Informations de livraison:
ECCN:
Informations PCN:
Update!!!The previous official document 430-21018 notifying Toray Corporation of whether the UL certification was unqualified was confirmed as follows: 1. Announcement from Toray (1) For all applicable materials for which inappropriate acts were made in FUS (follow-up service) in the past, it has been decided that the existing UL certification registration is unchanged as it is.(2) Even for grades for which inappropriate acts were not made, UL certification registration is unchanged as it is. 2. Impact on HiroseAs UL certification registration of Amilan/TORAYCON is unchanged, there is no impact on UL certification registration of our products using Amilan/TORAYCON.We continue to supply our products using the applicable materials.
UPDATE to previous PCN 88110..Impact on our products by Inappropriate Identification on Nylon resin Amilan and PBT resin TORAYCON of Toray Industries, Inc. Toray Industries, Inc. (Hereinafter Toray) announced followings about Nylon resin Amilan and PBT resin TORAYCON (Hereafter Applicable materials) that were improperly identified as receiving certification from Underwriters Laboratories, a third-party safety science organization in the United States (hereinafter, "UL"). We are writing to inform you of the impact on our products. 1 Announcement from Toray As a result of discussions between UL and Toray regarding the handling of UL certified applicable materials, Toray received the following conclusion from UL. (1) For all applicable materials for which inappropriate actions were made in FUS (follow-up service) in the past, it has been decided that the existing UL certification registration continues as it is. (2) Even for grades for which inappropriate actions were not made, UL certification registration continues as it is. Impact on our products:From the announcement from Toray that the UL certification registration of the applicable materials continues, there is no impact on UL certification registration of our products using the applicable materials.
Impact on our products by Inappropriate Identification of Toray Industries, Inc., Certain Resin, as Receiving Certification from Third Party OrganizationRecently, Toray Industries, Inc.,(Hereinafter Toray) announced that certain resin products were improperly identified by Toray as receiving certification from Underwriters Laboratories (hereinafter, "UL").We are writing to inform you of the impact on our company and our actions.UL recognition:At this moment, UL recognition of Toray's concerned resin was not canceled.
Recently, Toray Industries, Inc.,(Hereinafter Toray) announced that certain resin products were improperly identified by Toray as receiving certification from Underwriters Laboratories (hereinafter, "UL").We are writing to inform you of the impact on our company and our actions.1 Our impacted products Please refer to attached sheet.2 UL recognition At this moment, UL recognition of Toray's concerned resin was not canceled.3 Toray explanation to our company at this moment. Information on the inappropriate listing to UL registration of Toray is as follows. Some resin's samples submitted to UL for testing were different than the resins certified by UL. Some resins which were different than the composition certified by UL and that we manufactured and sold. Toray reported this matter to UL headquarters in the United States and been consulting with them toward future action. Toray has been evaluating the concerned resin which delivered to our company. But we have not received any reports from Toray that it affects the flamability grade.4. Shipment We continue to receive orders and shipping the impacted product.
Statut du produit:
Hirose Electric LF07WBJ-6S - Caractéristiques techniques
Type: | CPC-Connector |
Style/Orientation: | Free Hanging Receptacle |
No of Positions: | 6 |
Mating Type: | Push Pull |
Termination: | Male/Pin Solder |
IP Rating: | IP68 |
Voltage Rating: | 42V |
Current Rating: | 2A |
Operating Temp Range: | -25°C to +85°C |
Méthode de montage : | Wire Mount |
Emballages disponibles
Qté d'emballage(s) :
1 par Tray
Méthode de montage :
Wire Mount