FTM / Security & Encryption / Littelfuse — LS0504EDD12 eFuse
The Littelfuse LS0504EDD12 is a compact load switch which provides circuits with protection against over-current, over-voltage, over-temperature events, as well as limiting inrush current.
Featuring low on-resistance of 26 mΩ and low shut-down current, the LS0504EDD12 is ideal for applications that require both robust protection and low power consumption.
The LS0504EDD12 provides an accurate 1.2 V enable threshold that allows designers to set the under-voltage lockout (UVLO) limit through an external resistor-divider network. It has a built-in 8 Ω resistor for quick output discharge when disabled.
Other new additions to the Littelfuse portfolio of protection ICs are:
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility