FTM / Power & Power Management / DIODES™ — AS2376Q Op Amp
Diodes Incorporated has introduced the AS2376Q, a precision operational amplifier for automotive systems. The device is ideal for the signal conditioning circuit in applications that operate at high frequency, such as on-board chargers and dc-dc converters.
Featuring a gain-bandwidth product of 5.5 MHz, the AS2376Q op amp can handle signals at frequencies as high as 50 kHz without significant loss of accuracy. At the same time, low input-noise density of 9.5 nV/√Hz and 0.8 µVp-p low-frequency noise mean that the AS2376Q maintains good signal integrity.
The offset voltage is a low 5 μV, a value which allows the AS2376Q to provide a wide dynamic range.
The AS2376Q is manufactured in IATF 16949-certified facilities, and supports PPAP documentation.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility