FTM / Intelligent Sensing / STMicroelectronics — LSM6DSV16X IMU
STMicroelectronics has introduced the LSM6DSV16X, a six-axis inertial measurement unit (IMU) which features advanced artificial intelligence (AI) capabilities to bring smart motion-sensing capabilities to IoT devices at the edge of the network.
The device is ideal for functions such as motion tracking and gesture detection, indoor navigation, image stabilization, and vibration monitoring and compensation.
The LSM6DSV16X includes standard IMU components: a three-axis digital accelerometer and a three-axis digital gyroscope. But on top of this, ST has built in a triple core for processing acceleration and angular rate data on three separate channels, the user interface, optical image stabilization, and electronic image stabilization, with dedicated configuration, processing, and filtering functions.
The LSM6DSV16X’s AI capabilities also enable it to apply edge computing functions to the raw motion data that it captures. Its finite state machine (FSM) performs configurable motion tracking, while a machine learning core (MLC) supplies context awareness, and provides exportable AI features for IoT applications.
The LSM6DSV16X supports the adaptive self-configuration feature, which allows the FSM to automatically reconfigure the device in real time based on the detection of a specific motion pattern. Reconfiguration can also be driven by the output of a specific decision tree configured in the MLC, without any intervention from the host processor.
The LSM6DSV16X embeds ST’s new Qvar function, which detects variation in electric charge, for user interface functions such as tap, double-tap, triple-tap, long press, or L/R or R/L swipe.
The LSM6DSV16X features an analog hub which can interface to an external analog input and convert it to a digital signal for processing.
The STEVAL-MKI227KA evaluation kit is based on the LSM6DSV16X inertial module. It provides a Qvar electrostatic sensor, and three electrodes supporting finger swipe and generic functions. It is compatible with the STEVAL-MKI109V3 microcontroller motherboard.
It is possible to configure the LSM6DSV16X by changing the position of the jumper. The kit supports the entire LSM6DSV16X pinout, and comes ready-to-use with the required decoupling capacitors on the power-supply line.
The STEVAL-MKE00xAA can be plugged onto the STEVAL-MKI227A board. This adapter is supported by the STEVAL-MKI109V3 motherboard, which includes a high-performance 32-bit MCU functioning as a bridge between the sensor and a PC, on which it is possible to use the downloadable graphical user interface Unico-GUI, or dedicated software routines for customized applications.
It is also possible to plug the board onto the X-NUCLEO-IKS01A3 expansion board.
Sign up for access to exclusive development boards, an essential tool for many innovative design projects.
*Available to pre-qualified EMEA customers only.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility