FTM / Intelligent Lighting / TE Connectivity — LUMAWISE Endurance S Connector System
The TE Connectivity (TE) LUMAWISE Endurance S connector system is a complete set of products for connecting light sensors and networked lighting controls in streetlights and area lighting.
There are two main offerings in the Endurance S family:
The LUMAWISE Endurance S system includes a receptacle, mounted to a street or area light fixture, as well as several bases and domes that together form a robust enclosure for connecting sensor modules and networked lighting controls.
The compact design is resistant to ultraviolet radiation and is IP66-rated. The connector can be mounted on the top, bottom or side of a luminaire.
TE has also extended the Endurance S portfolio with an S2 receptacle. Offered in both Zhaga Book 18- and Z10-enabled keyed varieties, the S2 receptacle provides two wires per contact. This makes for easier wiring and applied cost savings in luminaires that have a dual-node architecture.
TE Connectivity, LUMAWISE, TE and TE connectivity (logo) are trademarks.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility