FTM / Intelligent Lighting / Littelfuse — SSA Series Current Shunt Resistors
The new SSA series of two-terminal, ultra low-resistance shunt resistors from Littelfuse meets the growing demand for accurate current measurement in high-performance applications.
Compared to competing technologies such as Hall-effect sensors, current transformers, fluxgate sensors, and Rogowski coils, the Littelfuse current shunt resistor offers a more efficient and lower-cost solution, and one that works well in both ac and dc circuits. The SSA series also has a higher power rating than metal foil resistors.
The resistance of the SSA series is consistent and stable across production batches and temperature. Tolerance of resistance is as low as ±1.0%, and the temperature coefficient of resistance is as low as ±50 ppm/°C.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility