New Arm Cortex-M85-based devices bridge gap between MCUs and MPUs

The Renesas RA8 series microcontrollers feature Arm® Helium™ technology which boosts the performance of DSP functions and of AI and machine learning algorithms. The new MCUs also provide a rich set of security features including cryptographic acceleration and secure boot.

Renesas has introduced what it bills as the world’s most powerful microcontrollers. The new RA8 series MCUs, the industry’s first to implement the Arm Cortex®-M85 processor, produce industry-leading performance measured at 3,000 CoreMark points, or 6.39 CoreMark points/MHz. 

 

The deterministic, low-latency, real-time operation enabled by this high performance allows system designers to use an RA MCU in applications that would previously have required a microprocessor. The new RA8 series is part of the Renesas RA family of MCUs based on Cortex-M processors. Existing designs built for other RA devices can easily be ported to the new RA8 devices. 

 

The new RA8 MCUs deploy Arm Helium technology, which provides up to a four times improvement in DSP and machine learning performance compared to MCUs based on the Cortex-M7 processor. This performance boost can enable designers to eliminate an additional DSP in some systems.  

 

The combination of high CPU performance and Helium technology also provides a dramatic improvement in the MCUs’ ability to perform AI and machine learning tasks. For instance, the RA8 series MCUs enable edge and endpoint devices to implement natural language processing in voice AI and predictive maintenance applications, using Helium to accelerate neural network processing. The design of AI applications is assisted by Renesas’ embedded AI and TinyML solutions for automotive, industrial and commercial products, based on its Reality AI tools.  

 

The security of AI and connected devices benefits from the advanced features of the RA8 series MCUs. The Cortex-M85 core includes Arm TrustZone® technology, which enables isolation and secure/non-secure partitioning of memory, peripherals and code. The MCUs also feature the most advanced Renesas security IP, RSIP-E51A, which provides leading-edge cryptographic accelerators and supports a true secure boot.  

 

The RA8 series consists of the RA8M1 and RA8D1 groups. The RA8M1 are general-purpose MCUs that address diverse compute-intensive applications in industrial automation, home appliances, smart home, consumer, building/home automation, medical and AI applications. 

 

The RA8D1 MCUs are specialized with a feature set optimized for human-machine interface, graphics, and vision AI systems in the industrial automation, home appliances, smart home, consumer, home and building automation, and medical/healthcare market segments.  

 

All RA8 MCUs are supported by the Renesas Flexible Software Package (FSP). The FSP enables faster application development by providing all the infrastructure software needed, including multiple real-time operating systems, a board support package, peripheral drivers, middleware, and connectivity, networking, and security stacks. It also includes reference software for building complex AI, motor control and cloud designs.  

Features

  • Memory resources: 
    • Up to 2 Mbytes of Flash memory  
    • 1 Mbyte of SRAM, of which 512 kbytes are ECC protected 
    • Octal SPI Flash interface 
  • Interfaces:  
    • CAN-FD  
    • Ethernet 
    • Full-speed/Hi-Speed USB  
    • 16-bit camera interface 
    • I3C  
  • Security features: 
    • Cryptographic algorithms 
    • Immutable storage 
    • Tamper resistance with protection against side-channel attack  
    • Secure debug 
    • Secure factory programming  
    • Lifecycle management support 

Applications

  • Fingerprint scanners 
  • Thermostats 
  • Programmable logic controllers  
  • Smart meters  
  • Home hubs 
  • Industrial HMI 
  • Video doorbells 
  • Patient monitors 
  • Graphics calculators 
  • Security panels with displays 
  • Printer display panels 
  • Appliances 

Evaluation Kit

Part supported: RA8M1 group microcontrollers 

Kit part number: RTK7EKA8M1S00001BE 

Board Club search term: microcontrollers 

The RA8M1 group evaluation kit enables designers to easily evaluate key features of the RA8M1 MCU and develop sophisticated IoT and embedded systems applications.  

 

The kit supports on-board debugging using a SEGGER-J-Link® debugger.  

FTM Board Club

Sign up for access to exclusive development boards, an essential tool for many innovative design projects.

*Available to pre-qualified EMEA customers only.

Extra_Renesas_RA8_Series

Related Articles

Susumu — HRG Series of High-Power Chip Resistors
15 February 2024
Susumu HRG Series resistors feature high-power, precision and stable resistance over a wide temperature...
Read More
STMicroelectronics — STSAFE-A110 Secure Element
01 August 2024
This STSAFE-A110 Secure Element by STMicroelectronics provides a certified solution for asset authentication...
Read More
Monolithic Power Systems — Power Inductors
15 February 2024
Discover the wide range of Monolithic Power Systems Power Inductors for applications which include power...
Read More

Subscribe to our newsletters

Subscribe to Future Electronics

Get access to the latest product information, technical analysis, design notes and more

Choose your region