FTM / Embedded Processing and Software / Hirose Electric — FH72 Series FPC Connector
The new Hirose Electric FH72 series of flexible printed circuit (FPC) connectors is designed for quick, fail-safe installation in space-constrained applications.
With a contact pitch of just 0.3 mm and a height of 0.9 mm, this compact connector is suitable for small applications where space on the board is at a premium.
The unique one-action lock on the FH72 series allows an FPC to be locked into place simply by inserting it. This locking mechanism and the connector’s wide entry point make it possible for the FPC to be inserted with one hand or by automated machinery. This reduces both assembly time and the chance of mating failure that may be caused by movement involved in a two-step locking process.
Once in place, the high retention force achieved by the lock levers at either end of the connector ensures the tabbed FPC is held securely in the correct position. The correct placement of the FPC can be checked through small openings in the top of the connector.
The integral molding structure of the FH72 series leaves no gaps for solder wicking.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility