FTM / Connectivity / Renesas — Smart Lock System Design
Renesas is enabling OEMs to accelerate the development of products in fast-growing markets with the release of a series of system design blueprints combining embedded processing, analog, power, and connectivity components. These system elements draw on products from Renesas and Dialog Semiconductor, a Renesas company.
An example of these ‘Winning Combination’ system designs is a Smart Lock with Super Low-Power Wi-Fi and BLE, a popular application in home and building automation. A smart lock requires a method of user authentication and control via fingerprint recognition or a mobile phone, and to communicate with cloud services using a common wireless interface such as Bluetooth® or Wi-Fi® networking.
The Smart Lock Winning Combination implements these functions and more. For wireless connectivity, it features a DA16600 low-power Wi-Fi and Bluetooth Low Energy (LE) module. Designers could instead use a DA16200 low-power Wi-Fi networking system-on-chip (SoC) and/or a DA14531 SmartBond TINY™ Bluetooth LE module. Cloud connectivity can alternatively be provided by an RYZ014A LTE Cat-M1 cellular networking module.
The GreenPAK™ family of programmable devices performs functions such as a motor driver for operating the lock mechanism – the SLG47105 is ideal – and LED control for a simple user interface alongside a DA7280 haptic driver.
The Renesas RX651 32-bit microcontroller is the ideal option for running the algorithm for fingerprint recognition in a fingerprint sensing module. In addition, a Renesas ISL29501 time-of-flight sensor implements proximity sensing, to wake up the smart lock when a user is present.
Share This
Get access to the latest product information, technical analysis, design notes and more
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility