FTM / Connectivity / onsemi — NCN26010 Ethernet Controller
Factories today commonly use Ethernet networks for supervisory control and station management, but still rely on legacy fieldbus solutions to communicate with field instrumentation. Such legacy protocols need to be replaced and modernized with low-cost, single unshielded-pair Ethernet solutions which will allow factories to run data over Ethernet seamlessly from the cloud to the edge.
The IEEE 802.3cg standard provides a specification for the technology to overcome the gap in industrial Ethernet systems, offering low-cost communication to field devices at a data rate of 10 Mbits/s using two new physical layers:
The NCN26010 from onsemi, one of the first 802.3cg-compliant 10BASE-T1S Ethernet controllers, provides a reliable way to take advantage of the benefits of single-pair Ethernet technology.
The NCN26010’s noise immunity is far higher than is specified in the 10BASE-T1S standard: a proprietary enhanced noise immunity feature provides robust signal detection in noisy industrial environments, and can extend the network range to up to 50 m.
The NCN26010 also offers very low line capacitance, enabling it to support five times the node requirement of the IEEE 802.3cg standard, up to 40 nodes on a 25 m segment. This helps factory operators to save more on the cost of wiring and installation.
Multi-drop Ethernet offers a way to reduce the wiring and installation costs which typically dominate the networking budget in many factories: a network can be completed with up to 70% fewer cables while reducing installation costs by as much as 80%. 10BASE-T1S also offers the flexibility to repurpose nodes after the initial installation.
Additional benefits include:
Part Number: NCN26010XMNEVK
The NCN26010XMNEVK demonstrates the basic functionality of the NCN26010 MAC and transceiver, and doubles as a laboratory tool to allow engineers to develop their own embedded software drivers for the NCN26010 device.
The evaluation kit consists of the NCN26010BMNEVB bridge board and the NCN26010XMNEVB 10BASE-T1S evaluation board.
Sign up for access to exclusive development boards, an essential tool for many innovative design projects.
*Available to pre-qualified EMEA customers only.
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2025 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility