FTM / Connectivity / Nexperia — NXU0304 4-bit Translators
The NXU0304 voltage-level translating buffer ICs are the latest devices in the cost-effective NXU family from Nexperia. The NXU translators cover 4-, 2-, and 1-bit operations to solve I/O level mismatches between system components that use common interface standards such as I2C, SPI, UART, JTAG, RMII and GPIO.
The wide voltage range of the NXU0304 level shifters offers increased flexibility for designers building systems with many different I/O voltages. This reduces the requirement for compromises in cost- and space-constrained designs, and eases integration of the most suitable components for the application. The high maximum data rate of the NXU0304 also enables interfacing with leading peripheral and host devices.
The NXU family offers multiple channel direction configurations for optimized operation and reduced system complexity. This means that the NXU translators have a lower pin count than direction-controlled translator ICs, and this enables smaller package sizes for more compact designs.
NXU0304
NUX0104
NXU0204
NXU0101
NXU0102
NXU0102
Be at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2024 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility